Connecting a GA800, FP605, GA500, or HV600 Drive to a PC
Topic Description

GA800, FP605, GA500, and HV600 drives have the capability to connect to a PC for use with DriveWizard software. There are a few different methods that can be used to make the initial connection.

After opening DriveWizard, the Drive Selection & Communication Setup window will have Serial / USB, Ethernet, or Bluetooth as the connection type shown below.

Note: GA800, FP605, GA500, and HV600 drives are also compatible with DriveWizard Mobile. Refer to the following document for more information: Obtaining, Installing, and Using DriveWizard Mobile.


Resolution

Serial / USB Connection Method

The serial or USB connection is a hard-wired, direct connection from a PC to a drive requiring one of the following cables:

Note: For more information on these cables and their pinouts, refer to the following document: Difference Between PC Communications, Flash Cables, and Mobile Device Interface Cables.

Cable Type Connection Type Part Number Picture
USB Cable (Type A to Mini-B) USB UWR01258
Blue Serial Cable (no DIP switch) Serial  UWR00468-2 
Blue Serial Cable (with DIP switch) Serial UWR00468-1
Green Serial Cable (with DIP switches)  Serial UWR01076-1

For a serial-type connection, remove the keypad and connect one end of the serial cable to the RJ-45 port of the drive and the other end to a PC. A serial-to-USB converter may be required if the PC does not have a serial port. Yaskawa does not supply serial-to-USB converters.

For a USB-type connection, remove the rubber insert for the USB Mini-B port and connect one end of the USB cable to the USB Mini-B port of the drive and the other end to a PC.

Note: If a USB cable other than part # UWR01258 is being used, it is recommended the connectors have shielded wires.

For setup, open the Communication Setup tab in the Drive Selection / Communication Setup window.

  • For a serial-type connection, select Direct link (RS422 / RS485) as the connection type and choose the appropriate communications port (comm port) being used. For example, select "Com6" if that is the port being used.
    • Note: The comm port being used can be seen in Device Manager when connected to a drive.
  • For a USB-type connection, select Direct link (Operator / RS232 / USB Converter / direct USB). There are no further settings to change.

Note: The remaining default settings are generally sufficient for communication.

 

Ethernet Connection Method

The ethernet connection is used for communicating over a network via Ethernet/IP, Modbus TCP/IP, or Profinet communications. The drive must be using one of the following option cards for network communication and be on the same network as the PC.

Protocol Option Card Part Number
Ethernet/IP SI-EN3 (single port) or
SI-EN3D (dual port)
Modbus TCP/IP SI-EM3 (single port) or
SI-EM3D (dual port)
Profinet SI-EP3

For setup, open the Communication Setup tab in the Drive Selection / Communication Setup window. Select the appropriate network adapter and enter the drive's IP address. Refer to the following document if multiple network adapters are used on the network: Connecting to DriveWizard over Ethernet/IP or Modbus TCP/IP with Multiple Network Adapters.

 

Bluetooth Connection Method

The Bluetooth connection can be used to communicate from a PC to a drive via Bluetooth. The following optional keypads are required for a Bluetooth connection to a PC.

Drives GA800, FP605, GA500 HV600
Yaskawa Part # JVOP-KPLCC04MBB JVOP-KPLCD04ABB
Description Optional, Bluetooth, Backlit, Industrial Keypad with Lo/Re, RUN, STOP Keys Optional, Bluetooth, Backlit, HOA Keypad with HAND, OFF, AUTO Keys
Image

For setup, open the Communication Setup tab in the Drive Selection / Communication Setup window. Enter the Bluetooth ID to match the parameter A1-12 (range: 0000 - 9999) which must be set in the drive to enable the Bluetooth capabilities.


Related Documents
Connecting to a GA800, FP605, GA500, or HV600 Drive using DriveWizard Mobile USB OTG (On-The-Go) With or Without Main Power
Enabling Bluetooth Capability on the Optional Bluetooth Keypad for a GA800, FP605, GA500, or HV600 Drive
GA800, FP605, GA500, and HV600 LCD Keypad Part Numbers
Obtaining, Installing, and Using DriveWizard HVAC Software
Obtaining, Installing, and Using DriveWizard Mobile
Obtaining, Installing and Using DriveWizard Industrial Software

Product Types
FP605, GA800, GA800 Configured, GA500, HV600, HV600 Bypass, HV600 Configured, HV600 Redundant,
All Applications
Advanced Random Rotary Knife with Cam Blend, Air Compressor, Blister pack Thermoformer, Cartoner, Centrifuge, Conveyor, Crane/Hoist, Dynamometer, Elevators and Escalators, Extrusion, Fans/Blowers, Feed To Length, General Machinery, HVAC, Irrigation, Labeler, Laundry, Linear Flying Shear, Machine Tool, Mixer, Other, Packaging, Palletizer, Precision Grinding, Pump, Punch Press, Rotary Knife, Rotary Placer, Rotary Table Indexer, Screw Feeder, Synch-Belt, Textile, Winding,
Option Types
DriveWizard Industrial, DriveWizard HVAC, EtherNet for VFD, Modbus TCP/IP for VFD, Profinet for VFD, Digital Operator / Keypad with Bluetooth,
Last Modified Date: 02-03-2025ID: 13496