Topic Description
| |
|
The HV600 drive is set by default to automatically restart when power is lost momentarily or for an extended period of time and a RUN command is present. Under a certain circumstance, the drive may not automatically restart due to the built-in Real Time Clock resetting itself at every power-up (pictured below).
Note: The following parameters are set by default to allow the HV600 drive to automatically restart in AUTO and/or when a physical RUN command is present:
-
b1-17 = 1 (Allows the drive to accept an existing RUN command at power-up)
-
L2-01 = 2 (Allows the drive to ride through a momentary power loss as long as the CPU is active)
-
S5-10 = 2 (Keeps the AUTO mode status when the drive is de-energized)
|