NEMA 1 Configured Cabinets Without Motor Terminal Block
Topic Description

On certain A1000 and P1000 Configured units, on the NEMA 1 configured cabinets may NOT have a motor terminal block compared to previous version of the same cabinets.


Resolution

There was a new implementation made on the NEMA 1 configured cabinets containing the load reactor option. If the cabinet has a load reactor option, the motor connection points will be on the output side of the load reactor (see image below).

 

The previous motor connection point was on a terminal block (see image below).


Product Types
A1000 Configured, P1000 Configured,
All Applications
Advanced Random Rotary Knife with Cam Blend, Air Compressor, Blister pack Thermoformer, Cartoner, Centrifuge, Conveyor, Crane/Hoist, Dynamometer, Elevators and Escalators, Extrusion, Fans/Blowers, Feed To Length, General Machinery, HVAC, Irrigation, Labeler, Laundry, Linear Flying Shear, Machine Tool, Mixer, Other, Packaging, Palletizer, Precision Grinding, Pump, Punch Press, Rotary Knife, Rotary Placer, Rotary Table Indexer, Screw Feeder, Semiconductor, Solar Cell Tabbing and Bussing, Solar - Textured Etching, Synch-Belt, Textile, Winding,
Last Modified Date: 07-22-2024ID: 12930