Explicit Messaging vs Implicit Messaging on Yaskawa Drives |
|
||
Both explicit messaging and implicit messaging can be used on Yaskawa drives when using Ethernet IP communications. It is important to know when one method should be used over the other. Note: Not all 1000 series and 7 series drives are capable of Ethernet IP communications. |
|
||
Whether explicit messaging or implicit messaging should be used depends on the PLC or controller. Explicit Messaging - A type of messaging format that the user will poll as information is needed.
Implicit Messaging - A type of messaging format that is constantly sending information on a time interval, often referred to as polled messaging, meaning it is constantly sending information on a time interval. Which method can be used will depend on the PLC or controller since the drive can do both.
|
|
||
FP605, FP605 Bypass, FP605 Configured, GA800, GA800 Configured, GA500, HV600, HV600 Bypass, HV600 Configured, HV600 Redundant, A1000, AC7, A1000 Configured, E7, A1000 HHP, E7B Bypass, E1000, E7BR, H1000, E7BR Bypass Nema 3R, iQpump VTC, iQpump Micro-4X, iQpump Micro, iQpump1000, E7C Configured, iQpump1000 Bypass, E7CR, E7E Engineered, E7L Bypass, E7N Bypass, iQpump Micro Configured, E7S Slim Configured, F7, iQpump1000 Configured, iQrise, F7C Configured, J1000, FS7, L1000, G7, P1000, G7C Configured, P1000 Bypass, iQpump 7 Series, P1000 Configured, J7, U1000 Configured, U1000 Industrial, L7, U1000 Industrial Configured, U1000 iQpump, P7, U1000 iQpump Configured, P7BR, U1000L, P7 Bypass, U1000 Oil and Gas, P7C Configured, V1000, P7CR, V1000-4X, P7 Slim Configured, Z1000, PPBB, Z1000 Bypass, PPBR, Z1000 Configured, PPCB, Z1000 Redundant Bypass, PPCR, Z1000U, V7, Z1000U Bypass, V74X, V7C Configured, Z1000U Configured, V7CX Configured, V7N, V7N4X, |
|
||
Air Compressor, Cartoner, Centrifuge, Conveyor, Crane/Hoist, Dynamometer, Elevators and Escalators, Extrusion, Fans/Blowers, Feed To Length, General Machinery, HVAC, Irrigation, Labeler, Laundry, Linear Flying Shear, Machine Tool, Mixer, Other, Packaging, Palletizer, Precision Grinding, Pump, Punch Press, Rotary Knife, Rotary Placer, Rotary Table Indexer, Screw Feeder, Solar - Textured Etching, Synch-Belt, Textile, Winding, |
|
||
EtherNet for VFD, |
Last Modified Date: 03-07-2024ID: 12920 |
|