V1000 and V1000 4X Menu Functions With Video
Topic Description

The LED display and a description of the V1000 and V1000 4X menus are listed below. They can be accessed by pressing the up or down arrows after power-up.


Resolution
Power Up   This display screen allows the user to monitor and set the frequency reference while the drive is running.
Note: The user can select items to display when the drive is first powered up by setting parameter o1-02.
Drive Mode    
  "For" = Motor rotates forward
"rEv" = Motor rotates in reverse
   
  Monitors the frequency output by the drive.
   
  Monitors the output current of the drive.
   
  Scroll through o1-01 (User Monitor Selection) until the desired contents appear.
   
  Monitor parameters (U parameters) are displayed.
Programming Mode    
  Lists all parameters that have been edited or changed from default settings
   
  A select list of parameters necessary to get the drive operational quickly.
   
  Allows the user to access and edit all parameter settings.
   
  Motor parameters are calculated and set automatically.
   
Drive Mode   Returns to the frequency reference display screen

Yaskawa requests that viewers do not embed this video on other online articles or websites. To share this video, share a link to Yaskawa's Solution Center page containing the video.

 


Related Documents
Keypad Button Descriptions and Functions for 1000 Series Drives
Using the V1000 Digital Operator with Video

Product Types
V1000, V1000-4X,
All Applications
Advanced Random Rotary Knife with Cam Blend, Air Compressor, Blister pack Thermoformer, Cartoner, Centrifuge, Conveyor, Crane/Hoist, Dynamometer, Elevators and Escalators, Extrusion, Fans/Blowers, Feed To Length, General Machinery, HVAC, Irrigation, Labeler, Laundry, Linear Flying Shear, Machine Tool, Mixer, Other, Packaging, Palletizer, Precision Grinding, Pump, Punch Press, Rotary Knife, Rotary Placer, Rotary Table Indexer, Screw Feeder, Semiconductor, Solar Cell Tabbing and Bussing, Solar - Textured Etching, Synch-Belt, Textile, Winding,
Last Modified Date: 10-16-2024ID: 12371