Troubleshooting a CE (Communications Error) Fault on a Stand-Alone Drive (Non-Bypass)
Topic Description

A CE (Communications Error) fault indicates no control data was received from the connected PLC when using serial communications. Typically this fault occurs when a drive is communicating with a PLC via Modbus, BACnet MS/TP, Apogee, or Metasys and communication is lost for the duration of time set in parameter H5-09.

Note: A CE fault may often be referred to as a Serial Comm Error.


Resolution

Refer to the below recommendations when troubleshooting a CE (Communications Error) fault:


Related Documents
BACnet MS/TP, Modbus (RS-485), Apogee, and Metasys Communication Wiring, Recommended Shield Termination Points and Sudden Loss of Communication
EMC Filter grounding
Modbus, Metasys, Apogee, and BACnet MS/TP Self-Diagnostic Test for HV600, FP605 and Z1000 Drives
Modbus Self-Diagnostic Test for GA500 Drives
MODBUS Self-Diagnostic Test for GA800, U1000, A1000, P1000, and iQpump1000 Drives
MODBUS Self-Diagnostic Test for V1000 and iQpump Micro Drives
Schaffner and Epcos EMC filters with Enclosure Rating
Setting the Stopping Method during a Communication Error (CE)
Troubleshooting a CALL Alarm
Troubleshooting a CE (Communications Error) Fault on a Z1000 Bypass, P1000 Bypass, or Z1000U Bypass
Warnings When Using an EMC Filter with Yaskawa Drives

Product Types
FP605, GA800, GA800 Configured, GA500, HV600, HV600 Configured, A1000, A1000 Configured, A1000 HHP, E1000, H1000, iQpump VTC, iQpump Micro-4X, iQpump Micro, iQpump1000, iQpump1000 Bypass, iQpump Micro Configured, iQpump1000 Configured, iQrise, J1000, L1000, P1000, P1000 Bypass, P1000 Configured, U1000 Industrial, U1000 Industrial Configured, U1000 iQpump, U1000 iQpump Configured, U1000L, U1000 Oil and Gas, V1000, V1000-4X, Z1000, Z1000 Bypass, Z1000 Configured, Z1000 Redundant Bypass, Z1000U, Z1000U Bypass, Z1000U Configured,
All Applications
Advanced Random Rotary Knife with Cam Blend, Air Compressor, Blister pack Thermoformer, Cartoner, Centrifuge, Conveyor, Crane/Hoist, Dynamometer, Elevators and Escalators, Extrusion, Fans/Blowers, Feed To Length, General Machinery, HVAC, Irrigation, Labeler, Laundry, Linear Flying Shear, Machine Tool, Mixer, Other, Packaging, Palletizer, Precision Grinding, Pump, Punch Press, Rotary Knife, Rotary Placer, Rotary Table Indexer, Screw Feeder, Semiconductor, Solar Cell Tabbing and Bussing, Solar - Textured Etching, Synch-Belt, Textile, Winding,
Option Types
Apogee for VFD, BACnet MS/TP for VFD, Metasys for VFD, Modbus for VFD, Profibus for VFD,
Last Modified Date: 04-08-2025ID: 12343