Setting Up a Damper Actuator and End Switch for a GA800, GA500, A1000, or V1000 Drive
Topic Description

In many HVAC and fan applications, actuators are used to open and close dampers depending on the air flow. Often at times, it may be desired to use a damper end switch with a GA800, GA500, A1000, or V1000 drive. The following process allows for a (BAS) damper interlock circuit when a RUN command is present.

  1. A RUN command is issued to the drive (uses the Drive Enable function).
  2. A digital output (status of Drive Enable) will close a set of contacts and send a signal to the damper motor to open the damper.
  3. Once the damper reaches its end point, a set of damper contacts will close, sending a signal to the drive to start.

Resolution

Follow the steps below to setup a damper interlock circuit on a GA800, GA500, A1000, or V1000 drive.

Programming

  • Set parameter H1-0x = 6A (Drive Enable). This will correspond to the digital input terminal Sx used for the RUN command.
    • Example: If using terminal S3, set parameter H1-03 = 6A.
  • Set parameter H2-0x = 38 (Drive Enable). This will correspond to the digital output terminals Mx and My used for the damper motor.
    • Example (GA800/A1000): If using terminals M1/M2, set parameter H2-01 = 38.
    • Example (GA500/V1000): If using terminals MA/MC, set parameter H2-01 = 38.

Wiring

  • Wire the RUN command to terminals Sx and SN / SC. This is the digital input programmed for Drive Enable (H1-0x = 6A).
  • Wire the damper end switch to terminals S1 and SN / SC.
  • Wire the damper motor to terminals Mx and My. This is the digital output programmed for Drive Enable (H2-0x = 38)

See below for example wiring diagrams:

A1000 and GA800 Drives GA500 V1000
     

Note: The digital output terminals M1/M2 and MA/MC are rated for 30VDC or 250VAC, max 1A.


Related Documents
Setting Up a Damper Actuator and End Switch for a HV600 or Z1000 Drive

Product Types
GA800, GA800 Configured, GA500, A1000, A1000 Configured, V1000, V1000-4X,
All Applications
Air Compressor, Fans/Blowers, HVAC,
Last Modified Date: 05-20-2024ID: 11445