FB26 fault on a bypass panel with Bypass Software VST800400 or later with an option card mounted to CN5 of the drive
Topic Description

If an SI-xx option card is installed on the drive CN5 connector instead of on the bypass control board,  the frequency reference source is affected and the drive will not be able to communicate correctly to the bypass control board using MODBUS.

Therefore, an FB26 (Option on Drive) fault was added in software VST800400 for P1000 Bypass, Z1000U Bypass, Z1000 Bypass.


Resolution
  1. The option card must be removed from CN5 of the drive in order to reset the fault as shown:
  2. To use the option card, it should be mounted directly to terminal CN5 of the bypass control board.

Product Types
P1000 Bypass, Z1000 Bypass, Z1000U Bypass,
All Applications
Advanced Random Rotary Knife with Cam Blend, Air Compressor, Blister pack Thermoformer, Cartoner, Centrifuge, Conveyor, Crane/Hoist, Dynamometer, Elevators and Escalators, Extrusion, Fans/Blowers, Feed To Length, General Machinery, HVAC, Irrigation, Labeler, Laundry, Linear Flying Shear, Machine Tool, Mixer, Other, Packaging, Palletizer, Precision Grinding, Pump, Punch Press, Rotary Knife, Rotary Placer, Rotary Table Indexer, Screw Feeder, Semiconductor, Solar Cell Tabbing and Bussing, Solar - Textured Etching, Synch-Belt, Textile, Winding,
Option Types
Communications,
Last Modified Date: 07-22-2024ID: 11063