CN8 safety function operation and Pin out of CN8 on Sigma-5 and Sigma-7 SERVOPACKs |
|
||
The safety function or Hard Wire Base Block function (HBB) is designed to baseblock or shut off the motor current using the internal hardwired circuits connected to CN8. When there is a requirement to configure the safety function with multiple Sigma 5 SERVOPACKs, the safety function of Sigma 5 SERVOPACKs can be used with interlocking multiple drives so that all drives would display HBB when at least one of them has the safety input open. The SERVOPACK does not need to be enabled for the safety input to open and cause HBB to occur. . |
|
||
The safety should be wired in series so that safety protection is through all the devices that are requiring to be stopped in the event of a safety condition. New Part number of the cable is CVH03-03(A)-E (includes connector kit part number 2013595-1 made by manufacture Tyco Electronics AMP K. K.) This cable is sold in length from 0.45, and 1-12 meters. The "03" in the part number CVH03-03(A)-E represents the length and can be changed for the required length. A45 is the 0.45M cable. Note: The pin outs of CN8 connection can be found under Sigma 5 catalog towards the end of all amplifier sections. Note: It is the responsibility of the user to perform a Risk Assessment of the machine as a system. The safe-stop function embedded in the Sigma-5 SERVOPACK, when used with other safety components, provides protection according to EN954-1 Category 3 /IEC61508-1 to -4 SIL 2 for safe stop and protection against restart. The Sigma-5 SERVOPACK is just one component in a safety control system. To assure that the safe-stop function appropriately fulfills the safety requirements of the application, a thorough risk assessment must be done according to ISO 12100: "Safety of Machinery - General Principles for Design - Risk Assessment and Risk Reduction" for the whole safety system at the final installation. All components in the system must be appropriately selected and applied to achieve the desired safeguarding |
|
||
CN8 and Safety Option Module Details for 200v and 400v Sigma-5 and Sigma-7 SERVOPACKs
Safe Torque Off (STO) Example on Sigma 5 and Sigma 7 SERVOPACKs |
|
||
Sigma-7 Series, Sigma-5 Series, |
|
||
Advanced Random Rotary Knife with Cam Blend, Air Compressor, Blister pack Thermoformer, Cartoner, Centrifuge, Conveyor, Crane/Hoist, Dynamometer, Elevators and Escalators, Extrusion, Fans/Blowers, Feed To Length, General Machinery, HVAC, Irrigation, Labeler, Laundry, Linear Flying Shear, Machine Tool, Mixer, Other, Packaging, Palletizer, Precision Grinding, Pump, Punch Press, Rotary Knife, Rotary Placer, Rotary Table Indexer, Screw Feeder, Semiconductor, Solar Cell Tabbing and Bussing, Solar - Textured Etching, Synch-Belt, Textile, Winding, |
|
||
Functional Safety, |
Last Modified Date: 09-29-2022ID: 11053 |
|