Using a Drive on an Open Delta Power System |
|
||||||
An open delta power system is a power configuration using only two transformers instead of three to generate 3 phase power. In essence, one side of the secondary delta is physically missing but a 3-phase measurement is still possible phase to phase. This power configuration is not as efficient as a 3-transformer bank system but saves the consumer and utility company the cost of using one less transformer and is generally found at locations where the majority of the load uses single phase. As a result, an open-delta power system is not a true 3-phase balanced system and thus provides an unbalanced power supply. There are two key areas that are affected by the installation of a VFD on an open-delta power system:
Refer to document: PR.PS.01 for more information. It is important for a drive to be properly sized when used on an open-delta power system. The electrical diagrams below show a basic representation of the different types of an open delta power system.
|
|
||
Most* Yaskawa's VFDs are compatible with an open delta power system with an appropriate derate. It is best to speak with an outside sales rep for additional information. Alternatively, one of the methods below can be used when sizing a drive on an open-delta power system.
* Z1000, U1000, Z1000U, and U1000 iQpump drives are not compatible with an open delta power system as these require a balanced, 3 phase supply. Note: If an EMC filter is being used, it must be removed from the main circuitry or internally disabled (GA500 drives). |
|
||
All Drives, |
|
||
Advanced Random Rotary Knife with Cam Blend, Air Compressor, Blister pack Thermoformer, Cartoner, Centrifuge, Conveyor, Crane/Hoist, Dynamometer, Elevators and Escalators, Extrusion, Fans/Blowers, Feed To Length, General Machinery, HVAC, Irrigation, Labeler, Laundry, Linear Flying Shear, Machine Tool, Mixer, Other, Packaging, Palletizer, Precision Grinding, Pump, Punch Press, Rotary Knife, Rotary Placer, Rotary Table Indexer, Screw Feeder, Semiconductor, Solar Cell Tabbing and Bussing, Solar - Textured Etching, Synch-Belt, Textile, Winding, |
Last Modified Date: 07-11-2024![]() |
|