Using the Safe Disable Inputs (Safe Torque Off) |
|
||
The Safe Disable Inputs (H1, H2, HC) on GA800, GA500, HV600, FP605, A1000, U1000, and V1000 drives provide a stop function that complies with "Safe Torque Off" as specified by IEC/EN 61800-5-2:2007. Typically, these will be used as an emergency stop where the drive will immediately stop outputting to the motor. Note: V1000 drives only have a single input (H1) for the safe disable function. An additional option card is required for dual safe disable inputs: V1000 Dual Input Safe-Torque-Off Option
|
|
||
The diagrams below provide examples when using the Safe Disable Inputs.
GA800, HV600, FP605 and GA500 Drives (SINK mode) Example:
A1000 & U1000 Drives (SINK mode) Example:
V1000 Drives (SINK mode) Example:
|
|
||
FP605, GA800, GA800 Configured, GA500, HV600 Configured, A1000, A1000 Configured, U1000 Industrial, V1000, V1000-4X, |
|
||
Advanced Random Rotary Knife with Cam Blend, Air Compressor, Blister pack Thermoformer, Cartoner, Centrifuge, Conveyor, Crane/Hoist, Dynamometer, Elevators and Escalators, Extrusion, Fans/Blowers, Feed To Length, General Machinery, HVAC, Irrigation, Labeler, Laundry, Linear Flying Shear, Machine Tool, Mixer, Other, Packaging, Palletizer, Precision Grinding, Pump, Punch Press, Rotary Knife, Rotary Placer, Rotary Table Indexer, Screw Feeder, Semiconductor, Solar Cell Tabbing and Bussing, Solar - Textured Etching, Synch-Belt, Textile, Winding, |
Last Modified Date: 09-24-2024![]() |
|